|
 |
 |
 |
| Mitsubishi Electric's photovoltaic (PV) modules are an indispensable source of clean energy for the future. They help reduce the consumption of fossil fuels, and decrease negative impact on the planet. In some areas, electricity generated by PV can even be sold at a premium price. That's why these modules are used in an expanding number of public facilities, offices and homes throughout Europe and worldwide. |
 |
| Mitsubishi Electric's PV products are produced in Japan, at some of the company's most advanced integrated production facilities. The facilities are ISO 9001/14001 certified, with unique technologies and automated processes to ensure photovoltaic cells and modules of the highest possible quality. |
 |
Click here to find out more about Mitsubishi Electric solar power systems. Or click a country below to access the local website of the Mitsubishi Electric Europe branch office that handles photovoltaic systems.
> Italy |
 |
 |
 |
| Mitsubishi Electric has successfully produced the first cells in Japan that do not require solder coatings, a milestone in the development of environmentally friendly composite materials and manufacturing processes for the silver electrodes used on the surfaces of crystalline silicon photovoltaic cells. Our photovoltaic (PV) modules are now made using lead-free solder, eliminating lead from the manufacturing process. |
 |
| Mitsubishi Electric photovoltaic modules are designed for both commercial and domestic applications suitable for grid-connected systems, and offer both high performance and reliability. These polycrystalline PV modules are manufactured to the strictest engineering guidelines to meet the strict requirements of international quality standards (UL 1703, IEC 61215, TÜV Safety Class II). |
|
|
|
| Installation Examples |
 |
 |
 |
Commercial Use
Kindergarten
Italy
(14kW System) |
|
 |
 |
 |
Commercial Use
Small Power Plant
Austria
(400kW System) |
|
 |
 |
 |
Residential Use
Germany
(3kW System) |
|
|