Nocturnal Chants: Chisato Taniguchi’s Performance in Bassano
Italy / Culture
04 October 2024
Nocturnal Chant at San Bonaventura Church
Mitsubishi Electric Hydronics & IT Cooling Systems is proud of sponsoring Festival Cristofori which is a musical event in Padua, Italy dedicated to Bartolomeo Cristofori.
As part of our sponsorship of the Piano Festival B. Cristofori, they were delighted to include a special event in Bassano del Grappa within the CristOFF programme. This event showcased the celebrated Japanese pianist Chisato Taniguchi, born in 1998, renowned internationally for her unique fusion of classical and contemporary music. Remarkably, she had performed at the Venice Biennale just a day earlier.
On Friday, 4th October, at 8:45 PM, they had the honour of presenting her concert, Nocturnal Chants, in the atmospheric setting of San Bonaventura Church.
Chisato Taniguchi
They offered this remarkable musical evening as a gift not only to our employees but also to the entire community of Bassano del Grappa, where our headquarters is based. It was a celebration of art, culture, and our deep connection to the city, showcasing a world-class performance in a historic venue.
Presenting Flowers to Ms. Taniguchi
The concert programme included:
Ludwig van Beethoven: Sonata No. 32 in C minor op. 111
- Maestoso: Allegro con brio ed appassionato
- Arietta: Adagio molto semplice e cantabile
Atsuhiko Gondai: Rime dolenti op.191 – Sonnet for piano (Cristofori Festival Commission 2023)
Gabriel Fauré: Nocturnes Nos. 11 and 13
Claude Debussy: Images, Volume II
- Cloches à travers les feuilles
- Et la lune descend sur le temple qui fut
- Poissons d’or